This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2744: Restarting the MSP430 periodically

Part Number: MSP430G2744

Hi,

Is it possible to restart MSP430 at 50ms interval?
Our customer's application is battery powered and in order to save power
they are trying to Shutdown MSP430G2744 and start periodically instead of using standby mode.

Currently they are trying to restart at a 50ms interval but the MSP430 hangs up in between..
RST pin has 100kΩ+100nF in order to provide more delay during power-up.

Please let me know if this kind of usage is allowed with MSP430.

Best Regards
Kummi

**Attention** This is a public forum