This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR5739: using command line-flasher.exe runnin on WIN10

Part Number: MSP-EXP430FR5739
Other Parts Discussed in Thread: MSP-FET

Hi there!

For service I must reactive an older MSP-EXP430FR5739. For  the MSP-programming Eclipse & MSP-Toolchain is used as development-environment. These tools are on a VM with Debian 8. Everthing ist working well. Now I should ensure that the MSP-hex-binary  from a WIN 10 can be flashed into the board. I tried to do that with the command-line flasher. Before I had installed the TI-Usb-driver.The WIN device-manager
 has an COM-port MSP430 Application UART.

If I start the flasher, it shows the message:  Couldn't find any connected USB FETs!

By any chance has anybody a clue?

BergSchrat

**Attention** This is a public forum