This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds100v2 connection problem

Hi,

I have xds100v2 JTAG 14 pin connector and MSP432P401M microcontroller.I want to connect  XDS100V2 connector to MSP432P401M controller.

Below is design file of XDS100V2 connection to controller.

Can someone help me,

The connection is correct or not ?? Where the EMU0 and EMU1 pins of XDS100V2 JTAG connector are connected to controller??Should I left open these pins beacause there is no EMU0 and EMU1 pins on MSP432P401M controller.

**Attention** This is a public forum