Other Parts Discussed in Thread: MSP430F135, MSP430F1101A
Hi all
My design is a simple communication system with tx and Rx. I am transmitting data based on the key pressed on the remote. I have designed a look up table from which it picks up information based on th key pressed and transmits. On the receiving end, the same logic is being applied. M using MSP430F1101A for TX and MSP430F135 for RX.
The problem is that the system seems to be working fine most of the times but sometimes the output is random. I have to reset the system and start all over again for it to function normally. I feel that information in the look up table seems to be getting corrupted. And when i reset the system the correct information is being written back again. Thee application is very critical and cannot afford to malfunction so randomly.
PLease suggest on wht may be the exact problem and if possible some correction measures.
Help would be obliged
Regards