This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5131: Error compilation using IAR embedded workbench for msp430

Part Number: MSP430F5131

Tool/software: Code Composer Studio

Hello ,

I'm using IAR embedded workbench in order to program a msp430F5131 microcontroller.

although i get lots of error after i try to compile the code :

these are the errors i get :

main.c
Error[Pe101]: "CBCTL0_L" has already been declared in the current scope (at line 136 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 205
Error[Pe101]: "CBCTL0_H" has already been declared in the current scope (at line 137 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 205
Error[Pe101]: "CBCTL0" has already been declared in the current scope (at line 116 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 205
Error[Pe101]: "CBCTL1_L" has already been declared in the current scope (at line 177 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 207
Error[Pe101]: "CBCTL1_H" has already been declared in the current scope (at line 178 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 207
Error[Pe101]: "CBCTL1" has already been declared in the current scope (at line 156 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 207
Error[Pe101]: "CBCTL2_L" has already been declared in the current scope (at line 224 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 209
Error[Pe101]: "CBCTL2_H" has already been declared in the current scope (at line 225 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 209
Error[Pe101]: "CBCTL2" has already been declared in the current scope (at line 200 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 209
Error[Pe101]: "CBCTL3_L" has already been declared in the current scope (at line 274 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 211
Error[Pe101]: "CBCTL3_H" has already been declared in the current scope (at line 275 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 211
Error[Pe101]: "CBCTL3" has already been declared in the current scope (at line 250 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 211
Error[Pe101]: "CBINT_L" has already been declared in the current scope (at line 313 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 213
Error[Pe101]: "CBINT_H" has already been declared in the current scope (at line 314 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 213
Error[Pe101]: "CBINT" has already been declared in the current scope (at line 300 of "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\io430f5131.h") C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\430\inc\msp430f5131.h 213


Fatal Error[Ms016]: Error limit reached
Error while running C/C++ Compiler

Done. 101 error(s), 0 warning(s)

The code is :

#include "io430.h"
#include "msp430.h"
#include "intrinsics.h"
// defining flags as volatile(coz we use these variables in the main and in the ISR as well):
volatile unsigned int timerCount = 0; 	//defines the millisecond counter
volatile unsigned int normalPulse1=0; 	//defines another flag to indicates when 1 second has passed for normal pulse1
volatile unsigned int badPulse1=0;		//defines another flag to indicates when 1 second has passed for bad pulse1
volatile unsigned int normalPulse2=0; 	//defines another flag to indicates when 1 second has passed for normal pulse2
volatile unsigned int badPulse2=0;		//defines another flag to indicates when 1 second has passed for bad pulse2
volatile unsigned int secondsCount=0;	//defines the seconds count for the bad pulse


int main(void) { //Main function

	// configure watchdog timer:
	WDTCTL = WDTPW | WDTHOLD;					// Stop watchdog timer
	P2OUT &= ~(BIT4); 							//preload 1pps to '0'


	// set I/O pins directions:
	P1DIR |=BIT6+BIT7;                      //set p1.x to 11000000
	P2DIR |=BIT4;	                       // Set P2.4 to output direction
    PJDIR |=BIT0+BIT1+BIT3;                // set pj.x output 0000 1011
    P2SEL |= BIT4;						   //select the option of using TD0.0 in pin 2.4
    //P2IES |= BIT4;                         // high -> low is selected with IES.x = 1.
    //P2IFG &= ~(BIT4);                      // To prevent an immediate interrupt, clear the flag for
                                          // P2.4 before enabling the interrupt.
    //P2IE |= BIT4;                          // Enable interrupts for P2.4

    // Configure XT1 (external oscillator):
    PJSEL |= BIT4+BIT5;						// port select for xt1
    UCSCTL6 &= ~(XT1OFF); 				    //xt1 is on
    UCSCTL3 = 0;                            // FLL REFERENCE CLOCK REFERENCE = XT1

    // configure TD0.0 (TimerD0.0):
    TD0CTL0 |=MC_1+ID_3+TDSSEL_0+TDIE+CNTL_0+TDCLR;                //defining timer d TD0.0 (P2.4) upmode , devide by 8 , TDCLK , enable interupt , 
    TD0CCR0=1600-1;                          // setting TAR count up value 1600 (12.8MHz / 8 = 1.6MHz , 1.6MHz / 1600 = 1000 Hz) when 1000 is passed means 1 second has passed as well
	//TD0CCR1 =400-1;                           // setting the duty cycle to 25% pulse
    TD0CCTL0 |= CCIE;                        //ENABLES CCIFG INTERUPT ON CCR0
	//TD0CCTL1 |=CCIE;							//ENABLES CCIFG INTERUPT ON CCR1


    __enable_interrupt();    					//enables interupts in the ISR


    for(;;){                      // Main loop - Endless loop



    	//   EXTERNAL / INTERNAL SELECTION BY SW4

    	if ((P2IN & BIT2)==0){         //  INTERNAL MODE
		
    		PJOUT |=BIT3;              // sends '1' from pj.3 output to the multiplexer U4 (uses the internal 1pps)

    		//PULSE 1 : DESCRETE ON/OFF AND SWITCH ON/BAD/OFF

                     if ((P2IN & BIT0)==0 || (P1IN & BIT0)==0) {        //NORMAL SIGNAL OF 1PPS checks if descrete source is on or 1pps sw pulse 1 is on
                    	 P1OUT |= BIT6; 									//ENABLES PULSE BY THE 'AND' GATE
                    	 PJOUT |= BIT0;									//ENABLES TTL TO RS232 CONVERTER (FOR DIFF OUTPUT)
                          if(normalPulse1==1){                       //checks if normalPulse1 is on from the ISR
						    normalPulse1 =0;                           // sets normalPulse1 to 0 again so the ISR will generate the pulse 
						    P2OUT ^=BIT4;                            //generates 1pps out of p2.4
						 }

                	 }
                   
                     else {
                    	 P1OUT |= ~(BIT6); 								//DISABLES PULSE BY SENDING A '0' TO THE AND GATE
                     }

                     if ((P1IN & BIT2)==0)  {							//PULSE 1 BAD SIGNAL checks if the 1pps sw bad pulse is on
                    	  P1OUT |= BIT6; 									//ENABLES PULSE BY THE 'AND' GATE
                    	  PJOUT |= BIT0;									//ENABLES TTL TO RS232 CONVERTER (FOR DIFF OUTPUT)
						    if(badPulse1==1){                             //checks if badPulse1 is on from the ISR
							  badPulse1=0;                                // sets badPulse1 to 0 again so the ISR will generate the pulse
							  P2OUT ^=BIT4;                            //generates 1pps out of p2.4
							
							}
                     }

                     //PULSE 2 : DESCRETE ON/OFF AND SWITCH ON/BAD/OFF


                     if ((P2IN & BIT1)==0 || (P1IN & BIT0)==0){			//NORMAL SIGNAL OF 1PPS checks if descrete source is on or 1pps sw pulse 2 is on
                    	 P1OUT |= BIT7; 									//ENABLES PULSE BY THE 'AND' GATE
                    	 PJOUT |= BIT1;	 								//ENABLES TTL TO RS232 CONVERTER (FOR DIFF OUTPUT)
							if(normalPulse2==1){
								normalPulse2=0;								// sets normalPulse2 to 0 again so the ISR will generate the pulse
								P2OUT ^=BIT4;                            //generates 1pps out of p2.4
							
							}


                     }


    	
                     else {
                    	 P1OUT |= ~(BIT7);									//DISABLES PULSE BY SENDING A '0' TO THE AND GATE
                     }

                     if ((P1IN & BIT3)==0){								//PULSE 2 BAD SIGNAL 
                    	  P1OUT |= BIT6; 									//ENABLES PULSE BY THE 'AND' GATE
                    	  PJOUT |= BIT0;									//ENABLES TTL TO RS232 CONVERTER (FOR DIFF OUTPUT)
							if(badPulse2==1){
								badPulse2=0;								// sets badPulse2 to 0 again so the ISR will generate the pulse
								P2OUT ^=BIT4;                            //generates 1pps out of p2.4
							}
                     }


                     }

    	else {																//EXTERNAL MODE
    		PJOUT |= ~(BIT3);            //sends '0' from pj.3 output to the multiplexer U4 (uses the external 1pps)
    		P1OUT |= BIT6;      			// ENABLES PULSE 1
    		P1OUT |= BIT7;				//ENABLES PULSE 2
    		PJOUT |= BIT0;				//ENABLES RS422 DIFF OUTPUT	FOR PULSE 1
    		PJOUT |= BIT1;				// ENABLES RS422 DIFF OUTPUT FOR PULSE 2
    	    	}
    	}
		return 0;
}

	
	
                    //ISR FOR TIMERD0.0 - NORMAL/BAD PULSE 1 AND 2
					
					
					
					#pragma vector = TIMER0_D0_VECTOR 				//GENERATES 1PPS EVERY 1s for normal pulse
                   __interrupt void TIMER0_D0 (void){
					   
					   //NORMAL PULSE 1 AND 2:
					   
                	   if (++timerCount > 500) {   						// checks if the incrementation of timerCount reaches 500 (means 1 second has passed)toggling means doubling the time this is why we need to devide the time to a half. (1000/2=500)
					                       timerCount = 0;             // resets the millisecond counter to 0
										   normalPulse1 = 1;             //once it reaches 500 (1 second) normalPulse1 will be 1 
										   normalPulse2 = 1;				//once it reaches 500 (1 second) normalPulse2 will be 1 
										   secondsCount++;
                	                  	   }
                	                  	  
                     
					// BAD PULSE 1 AND 2:
					
				
                	   if (secondCount == 2) {   						// checks if the incrementation of secondCount reaches 2 seconds for bad pulse (means 2 second has passed)
											secondsCount = 0;             // resets the millisecond counter to 0
											badPulse1=1;					// once it reaches 2000( 2 seconds) the badPulse1 will be 1.
											badPulse2=1;					// once it reaches 2000( 2 seconds) the badPulse2 will be 1.
                	                  	   }
                	                  	   
}

  • Hi Omer,

    These errors mean that you have multiple definitions of the same name. Most likely io430.h is defining these variables and then msp430.h is redefining them. If you're not using anything from io430.h, comment it out and see if your code works.

    Best regards,
    Caleb Overbay

  • thank you that worked.

    i also wanna know , i have built and compiled the project without an error or warning . i would like to see the timeline simulation graph in IAR but it generates nothing.

    the project supposed to generate 1 pulse per second , how can i simulate it into a graph in the timeline?

    thanks in advance.

  • Hi Omer,

    I'm not too familiar with that feature but hopefully this guide helps you: Using Trace. I think you're looking for the SWO trace feature so I would start off with the "Getting Started with SWO Trace Section".

    I'm sorry I couldn't be of more help.

    Best regards, 
    Caleb Overbay

**Attention** This is a public forum