This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Hi guys,
I tried to use the Arduino library for MSP432 under Energia, but the error message attached below keeps showing up even I changed the board to MSP432 launchpad. So I wonder there might be something missing in the Energia compiler that hasn't been fully implemented for MSP432.
Please help me what can I do to make this happen. Thank you every one!
Jingyuan Liang
-----------------------------------------------------------------------Error Message-------------------------------------------------------------------------------------------------------------------
Energia: 1.6.10E18 (Windows 10), Board: "LaunchPad w/ msp432 EMT (48MHz)"
In file included from C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SystemInclude.h:23:0,
from C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h:26,
from C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdFat.h:27,
from E:\SdFat-master\SdFat-master\SdFat\examples\ReadWrite\ReadWrite.ino:24:
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/FatLib/SysCall.h: In static member function 'static void SysCall::yield()':
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/FatLib/SysCall.h:61:3: error: '::yield' has not been declared
::yield();
^
In file included from C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdFat.h:27:0,
from E:\SdFat-master\SdFat-master\SdFat\examples\ReadWrite\ReadWrite.ino:24:
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h: At global scope:
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h:52:52: error: 'SS' was not declared in this scope
bool begin(m_spi_t* spi, uint8_t chipSelectPin = SS,
^
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h:307:38: error: 'SS' was not declared in this scope
bool begin(uint8_t chipSelectPin = SS, uint8_t sckDivisor = 2) {
^
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h:315:61: error: 'SS' was not declared in this scope
bool init(uint8_t sckDivisor = 2, uint8_t chipSelectPin = SS) {
^
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdSpiCard/SdSpiCard.h:320:52: error: 'SS' was not declared in this scope
bool begin(m_spi_t* spi, uint8_t chipSelectPin = SS,
^
In file included from E:\SdFat-master\SdFat-master\SdFat\examples\ReadWrite\ReadWrite.ino:24:0:
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdFat.h:85:55: error: 'SS' was not declared in this scope
bool begin(SdSpiCard::m_spi_t* spi, uint8_t csPin = SS, uint8_t divisor = 2) {
^
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdFat.h:286:30: error: 'SS' was not declared in this scope
bool begin(uint8_t csPin = SS, uint8_t divisor = 2) {
^
C:\Users\Jingyuan\Documents\Energia\libraries\SdFat\src/SdFat.h:294:34: error: 'SS' was not declared in this scope
bool cardBegin(uint8_t csPin = SS, uint8_t divisor = 2) {
^
exit status 1
Error compiling for board LaunchPad w/ msp432 EMT (48MHz).
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
**Attention** This is a public forum