Part Number: MSP430FR5969
Dear Experts,
There is possibility to measure differential voltages with MSP430FR5969 ADC. Is it so that when ADC is used in differential mode, both inputs are still measured ground referenced and difference between two measurements is used as a differential result? The reason why I'm asking is because I'm not sure about the requirements for reference voltage in differential mode. Let's say I'm using ADC in differential mode and voltages are 3V and 2V, meaning that differential voltage is 1V. Do I still need reference voltage >3V, or is >1V enough?
Thanks!
Rgds,
Juha