This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F67471A: MSP430F67471A LCD Code Examples

Part Number: MSP430F67471A


Hello.

I have two questions.

 

  1. Should I clear REFMSTR bit in REFCTL register when I use LCD Controller with internal reference voltage?

   I also want to use ADC10.

   I understood REFMSTR must be set at all times when we use ADC10_A according to user guide page 695.

   But, in the sample code “msp430f677xA_lcdc_01.c”, REFMSTR is cleared.

 

2. If the answer of question.1 is “No”, how should I configure registers to generate internal voltage 2.96V in the

    sample code “msp430f677xA_lcdc_01.c”?

 

Regards,

Uchida-k

**Attention** This is a public forum