This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Different data from UART compare to Hyper terminal.



Tool/software: Code Composer Studio

Hi,

I suppose to get data 3b,82,53,81 but the data i get is 9b,82,2b,81 using uart what may the problem.

i had set uart configuration as below.

USCI/EUSCI:   USCI   EUSCI
Clock:                       32.768K                       1M                       1.048M                       4M                       4.194M                       8M                       8.388M                       12M                       16M                       16.777M                       20M                       Custom                   Hz
Baud rate:                       1200                       2400                       4800                       9600                       19200                       38400                       57600                       115200                       230400                       460800                       Custom                   bps
calculate

clockPrescalar:

firstModReg:

secondModReg:

overSampling:


Character frame is as show below.

     Start                          Parity             Next
             bit <----- 8 data bits -----> bit              Start bit
     Z   ____     ________________________________......______     __
             |   |  |  |  |  |  |  |  |  |  |                 |   |
     I/O     |   |ba|bb|bc|bd|be|bf|bg|bh|bi|     Guardtime   |   |
             |___|__|__|__|__|__|__|__|__|__|                 |___|_
     A       :   :                    :     :
             0   t1                   :    t10
             :                        :
             :<---- (n+/-0.2) etu --->:


                          Figure 3: Character frame

I hope data i have is enough for right communication but due some issue i couldn't  data as expected.

Thanks & regards

Praveen

**Attention** This is a public forum