This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC430F6147: Jitter on MCLK in frequency of 2.45MHz

Part Number: CC430F6147


Hi,

I took EVB of CC4306147 with code example that operate MCLK in 2.45MHz by external crystal 32.768KHz + FLL

and i have measured the MCLK by oscilloscope and i notice a jitter of 10nS, i have measured the the ACLK and the 32.768KHz is look very good.

Do you see any problem with the code?

Is this jitter is normal?

by the way i would like to work in MCLK of 4.194MHz for UART purpose (less error) , i have changed the code with 2 these lines marked in blue in the code, and i got 4.194MHz with jitter

is it OK ? or i need to change more value in the code

Thanks Hadi

 

 

see code below:

#include <msp430.h>

 

int main(void)

{

  WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer

 

  P1DIR |= BIT0;                            // P1.0 output

 

  PMAPPWD = 0x02D52;                        // Get write-access to port mapping regs

  P2MAP0 = PM_ACLK;                         // Map ACLK output to P2.0

  P2MAP2 = PM_MCLK;                         // Map MCLK output to P2.2

  PMAPPWD = 0;                              // Lock port mapping registers

 

  P2DIR |= BIT0 + BIT2;                     // ACLK, MCLK, SMCLK set out to pins

  P2SEL |= BIT0 + BIT2;                     // P2.0,2 for debugging purposes.

 

  // Initialize LFXT1

  P5SEL |= 0x03;                            // Select XT1

  UCSCTL6 |= XCAP_3;                        // Internal load cap

 

  // Loop until XT1 fault flag is cleared

  do

  {

    UCSCTL7 &= ~XT1LFOFFG;                  // Clear XT1 fault flags

  }while (UCSCTL7&XT1LFOFFG);               // Test XT1 fault flag

 

  // Initialize DCO to 2.45MHz

  __bis_SR_register(SCG0);                  // Disable the FLL control loop

  UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx

  UCSCTL1 = DCORSEL_3;                      // Set RSELx for DCO = 4.9 MHz

 UCSCTL2 = FLLD_1 + 74;                    // Set DCO Multiplier for 2.45MHz

 // UCSCTL2 = FLLD_1 + 127;                    // Set DCO Multiplier for 4.194MHz

                                            // (N + 1) * FLLRef = Fdco

                                            // (74 + 1) * 32768 = 2.45MHz

                                            // Set FLL Div = fDCOCLK/2

  __bic_SR_register(SCG0);                  // Enable the FLL control loop

 

  // Worst-case settling time for the DCO when the DCO range bits have been

  // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx

  // UG for optimization.

  // 32 x 32 x 2.45 MHz / 32,768 Hz = 76563 = MCLK cycles for DCO to settle

 __delay_cycles(76563);

 // __delay_cycles(131072);

 

  // Loop until XT1,XT2 & DCO fault flag is cleared

  do

  {

    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);

                                            // Clear XT2,XT1,DCO fault flags

    SFRIFG1 &= ~OFIFG;                      // Clear fault flags

  }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag

 

  while(1)

  {

    P1OUT ^= BIT0;                          // Toggle P1.0

    __delay_cycles(600000);                 // Delay

  }

}

  • Moving to MSP forum since this question is related to the MSP part and not the radio part
  • Hadi Shvartz said:
    and i have measured the MCLK by oscilloscope and i notice a jitter of 10nS, i have measured the the ACLK and the 32.768KHz is look very good.

    Jitter is expected in DCO output, unless modulator is off. Modulator switches between two discrete frequencies of DCO, resulting average frequency is determined by modulation bit counter. If you want clean msp430 clock, then XT2 high frequency crystal oscillator shall be used (on chips where it' s available).

**Attention** This is a public forum