Hello,
in the datasheet is a value stated for the settlingtime for the internal reference, if switched on. There is also a value stated for tON for the interal reference using in conjunction with the SD24. (I assume, the only difference is, that this are 2 different references. Settling and ON are meaning the same thing?!)
So, which time I'll have to wait, if I use an external reference? OK, it will also depend on the external circuit, but will there be times I'll have to consider, which will be "produces" inside the MSP?
BTW: tSETTLE is mentioned in the footer as tREFON. Typo?
Thanks in advance!
Regards,
Björn