Part Number: MSP430F6736A
Other Parts Discussed in Thread: MSP430AFE253, MSP-EXP430FR4133
Tool/software: Code Composer Studio
Dear colleagues,
I'm trying to program a MSP430F6736IPN (80 pins) using the spy-bi-wire interface from a MSP-EXP430G2 launchpad module with Code Composer Studio v6, but with no success. The launchpad module is working fine (I've tested it to program a MSP430AFE253 soldered in a separate board via SBW and it's OK), and the signal connections for SBW communication were made according to the rules suggested in the "MSP430 Hardware Tools" (SLAU278U). I also found other people that had the same trouble with this MCU - some of them employed a MSP-EXP430FR4133 launchpad instead of the MSP-EXP430G2. However, a friend told me that he managed to program a MSP430F6736IPZ (100 pins) using the MSP-EXP430G2 launchpad module. Has anyone here have the same issue? I'm planning to buy a MSP-EXP430FR4133 launchpad and try it to solve my problem, or (even better) a MSP-FET430UIF, but I would like to have some feedback and/or suggestions from anyone who has already have this problem.
Thanks!
Alex