This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5994: Compiler won't compile Audio Boosterpack with Sharp LCD example

Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP430WARE, , BOOSTXL-AUDIO

Tool/software: Code Composer Studio

I have installed the latest CCS, v.7, and I've used it sucessfully on other CPUs.  However, I'm interested in using the 5994 due to the built in silicon capable of FFT.  And so I got the whole Audio Development kit with the FR5994 SDK, the audio booster pack, and the LCD.  Hardware works because I'm able to run the App for temperature logging and see the board through the USB connection.

with that success, I dropped in the source code for the Audio Booster w Sharp 96x96 into my Workspace and imported it into CCS.  But I cannot compile it successfully. The place things explode first is when it reaches a .S43 file in one of the library directories.  I'm trying to get a default example to compile before I go any further in development, since knowing what to do and not to do is important.  Is there something I did incorrectly when I dropped the example folder into Workspace to compile it?

  • Hi Allen,

    I installed CCS v7, imported, and built the BOOSTXL-AUDIO_430BOOST-SHARP96_FFT_FIR_LEA_MSP430FR5994 project with no issues. Here are some screenshots that hopefully show how I did this. You may need to install MSP430Ware first, so that Resource Explorer can find it. I'm sure there are other methods, but this is the one I use primarily. Could you give this a try and let me know if your issue goes away?

    In Resource Explorer, I looked for the project and then clicked "Import to IDE" in the upper right.

    Next, I built the project.

    The build finished successfully.

    Regards,

    James

    MSP Customer Applications

  • Hi Allen,

    Did this resolve your issue?

    Regards,

    James

    MSP Customer Applications
  • Hi Allen,

    I'm closing this thread. Please feel free to reply back if you have any more related questions.

    Regards,

    James

    MSP Customer Applications

**Attention** This is a public forum