Part Number: MSP430F5636
Other Parts Discussed in Thread: MSP430F5659
Hello, we have a customer working on building of a slightly customised BSL for our MSP430F5636. This is based on the
MSP430BSL_1_00_12_00.zip
from http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSPBSL_CustomBSL430/latest/index_FDS.html
and was the starting point for this project.
The compiler version is IAR EW430 6.30. The customer can open the above and add some additional customization and this BSL works on the MSP-EXP430F5529LP however the same code does not function on the MSP430F5636 using the 100 pin socket board.
Next Step...
The default out-of-the-box compiled BSL project does not seem to work for MSP430F5636. Interestingly the BSL image that is provided by TI in precompiled form does work fine!
Can we have someone compile the above TI BSL source and test on the MSP430F5636 or MSP430F5659 on a 100 pin socket board, it may be that the linker command file is at fault.