Part Number: MSP430FR4133
I am using a MSP4320FR4133 and not setting the MCLK. But I do set the SMCLK at 1 MHZ for my SPI:
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
configRTCTimer();
P5SEL0 |= BIT0 | BIT1 | BIT2 | BIT3; // set 4-SPI pin as second function
UCB0CTLW0 |= UCSWRST; // **Put state machine in reset**
// 4-pin, 8-bit SPI master
UCB0CTLW0 |= UCMST|UCSYNC | UCMSB|UCMODE_2|UCSTEM;
// Clock polarity high, MSB
UCB0CTLW0 |= UCSSEL__SMCLK; // SMCLK
UCB0BR0 = 0x01; // /1,fBitClock = fBRCLK/(UCBRx+1) Clock at 1MHZ.
UCB0BR1 = 0; //
// UCB0MCTLW = 0; // No modulation
UCB0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCB0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
Does this a an effect on my MCLK? What would the MCLK frequency be?
Thanks