Hi,
today I tried to update my MSP Launchpad. The reason was I could not program a 2533 and my launchpad serial number is in between 1009xxxxx and 1101xxxxx. So i assumed the firmware is the reason. But an error occurred while using the LaunchPadFirmwareUpdater2.0.exe.
Win7 64bit
430g2231 connected
nothing else connected
But the update stopped with an error and now i cant even program the previous working microcontroller.
The Launchpad is not recognized from the CCS and the LaunchPadFirmwareUpdater2 is requesting a IC, but it is still in the socket.
Is my Launchpad now bricked?
Is there a way to restore it with another Launchpad or JTAG programmer?