This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5335: not generating correct pwm

Part Number: MSP430F5335

hii,

i have used msp430f5335 with 4 mhz external oscillator using timer B. i am getting pwm but not  worth of correct frequency. it is always showing (10^3)  less than actual value(using tektronix tds 2024c dso )

for ex :

  i wanted to get 5*(10^5) hz , but it is showing 5*(10^2) hz

i have written like this

#include "declare.h"
void gen_pwm()
{

WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P1DIR |= BIT0;
P4DIR |= BIT1;
P4SEL |= BIT1 ;

InitClocks();
TB0CTL =TBSSEL_1+ MC_1 +ID_3 ; 
TB0EX0 =TBIDEX_7;
// TB0CTL |=TBCLR;
TB0CCR0 =1000;
TB0CCTL1 = OUTMOD_7;
TB0CCR1 = 250;
TB0CTL |=TBCLR;

while(1);

}

i have written different function for clock generation. clock is working fine.

**Attention** This is a public forum