Part Number: MSP430F5659
Hi,
I am working on MSP430F5659 based controller with my custom board, using internal SMCLK 8MHz for CPU execution
I have membrane switch to turn ON-OFF. board.
Some time when i press the membrane switch system is not properly turning on ( No code runs) even micro-controller has the power i.e 3.3V,that is checked.
I don't know whether the Code Corruption is happening or reset vector corrupted , by the way wrong code execution during power is happening.
Any system power handling issue is causing this? since power is already available, or more current consumption by some external circuit causing this?
Since we have 24v generation logic, USB hub also present on our custom board.
How to make sure its due to reset vector corruption, any h/w issue, system voltage not properly handled ?
If i press again i.e. after 2-3 times system starts properly without any issue.
Please some one can help is resolving this issue, Thanks in advance
Nitesh