This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: Interfacing MSP430G2553 with Winbond SPI (W25Q80BV)

Part Number: MSP430G2553


Can anyone please help with how I can interface MSP430G2553 with Winbond SPI (W25Q80BV)? I am trying to use the USCI. I've tried on my own and have also tried referencing examples online but whenever I run in Debug mode the variable I defined to store the value coming back from the SPI just reads  255 '\xff'. Does anyone have working code that can help?

Here is the code I am using so far (keep in mind it is really not optimized as I just want to get something working):

#include "msp430g2553.h";

unsigned char addressValue;

/*
* main.c
*/
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer

initSPI();

addressValue = read(0x00);

while(1);

return 0;
}

// Configure MSP430 for SPI
/**
* Using UCA0
*
* MSP_PIN 1.1 = SPI_PIN 2 (Data Out)
* MSP_PIN 1.2 = SPI_PIN 5 (Data In)
* MSP_PIN 1.4 = SPI_PIN 6 (CLK)
* MSP_PIN 1.5 = SPI_PIN 1 (CS)
*
*/
void initSPI() {

// PIN Setup
P1OUT |= BIT5;
P1DIR |= BIT5;
P1SEL = BIT1 | BIT2 | BIT4;
P1SEL2 = BIT1 | BIT2 | BIT4;

/**
* Setup the UCACTL (UCA Control) Registers
* This sets the microcontroller to use SPI interface
*/
UCA0CTL1 = UCSWRST; // Reset mode
UCA0CTL0 |= UCCKPH + UCMSB + UCMST + UCSYNC; // 3-pin, 8-bit SPI Master (Most sig bit first)
UCA0CTL1 |= UCSSEL_2; // SMCLK

UCA0BR0 |= 0x02; // /2
UCA0BR1 = 0; //
UCA0MCTL = 0; // No modulation

UCA0CTL1 &= ~UCSWRST; // Initialize USCI state machine
}


unsigned char read(unsigned char regAddress) {

// CS High
//P1OUT |= BIT5;

// CS Low
P1OUT &= ~BIT5;

/**
* Send Read command to SPI
*/
while(!(IFG2 & UCA0TXIFG)); // TX BUFFER READY?
UCA0TXBUF = 0x03; // Tells SPI we want to do a read (03h)

/**
* Send Address where you wish to get data
*/
while(!(IFG2 & UCA0TXIFG)); // TX BUFFER READY?
UCA0TXBUF = regAddress;

int count;

/**
* Send dummy bits
*
*/
for(count = 0; count < 7; count++) {
while(!(IFG2 & UCA0TXIFG)); // TX BUFFER READY?
UCA0TXBUF = 0x00;
}

unsigned char result;

/**
* Read value from the SPI
*
*/
while(!(IFG2 & UCA0RXIFG)); // RX BUFFER READY?
result = UCA0RXBUF;

// Raise CS to Deselect drive
P1OUT |= BIT5;

return result;
}

// ************************* END CODE

Here is the SPEC for the Winbond SPI   https://cdn-shop.adafruit.com/datasheets/W25Q80BV.pdf

I took this next screenshot from the spec as it explains the SPI read process:

Finally - Here is a part of what I have stored on the SPI. My goal in the long run is to try and start with the first bit and read in each bit until I get to a certain length.

**Attention** This is a public forum