Hi All,
I would like to use the eZ430-RF2500 tool kit to manage inputs and outputs for 4 sensors under 500Hz sampling rate per each sensor (so all the 4 sensors should receive and give feed back 500 readings in each second)
there is another chip which generate the necessary analog input signals and capable of receiving the whole four sensors outputs (8kHz band width)
Can I use eZ430-RF2500 tool kit for this purpose?
Many thanks
Ali