Part Number: MSP430F6777
Other Parts Discussed in Thread: MSP430F6779
Hi,
I am evaluating MSP430F6777IPZ for our metering application. I have seen two flash banks available each of 128KB of size. We need to store the metering data in every 5 minute. Is it possible to use any one of the bank to store the metering data dynamically. Is it possible to write or read data from bank2 while the code is executing from the bank1. Is there any limitation for using the flash banks?
Is it support RS-485 2-wire half-duplex transmission interfacing, I have seen a few UARTs available in the data sheets
Also, is there a metering API library available for MSP430F6777IPZ. I have seen a few other chips having metering library supports
Thank you