Other Parts Discussed in Thread: ENERGIA
Hello all
As per the suggestions i am writing this post again
I am currently designing flow indicator totalizer for a company . I am working on msp430f5529 launch pad and trying to interfacr normal 16×2 lcd with it . I am using 2 softwares 1. Energia 1.6 2. Code composer studio v7
In energia as it is ready made library my lcd code is working perfectly well . But some times the software itself stucks and work stops
In CCS the library is not available or i cant find it out thus my simple lcd code is not working
Hard ware connections are
RS P3 BIT4
RW P3 BIT5
EN P3 BIT6
D4 P1 BIT2
D5 P1 BIT3
D6 P1 BIT4
D7 P1 BIT5
contrast is totally adjusted. Lcd is working fine tested on energia code
I am new at microcontroller programming so need assistance . In both the cases if anyone can resolve my problem with energia pls help .