Other Parts Discussed in Thread: CC1120, MSP430F5438A, BOOSTXL-CC1120-90
Tool/software: Code Composer Studio
Hi,
I would like to use LPM3 with port1/2 interrupts in MSP430F5529 LP together with 1120-1190 Booster pack using Sigfox library demo. I want MCU to go to lpm3 and only wake up with button Launchpad P1.1 and P2.1 interrupts and send Sigfox frames using library functions.
<Linking>
error #10056: symbol "__TI_int47" redefined: first defined in "./bsp/io_pin_int.obj"; redefined in "../ti_sigfox_library/TI_SIGFOX_lib_FCC.lib<hal_digio2.obj>"
error #10056: symbol "__TI_int42" redefined: first defined in "./bsp/io_pin_int.obj"; redefined in "../ti_sigfox_library/TI_SIGFOX_lib_FCC.lib<hal_digio2.obj>"
error #10010: errors encountered during linking; "TI_SIGFOX_FCC_ccs_project.out" not built