This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Upload code to MSP432 using UART

Part Number: MSP432P401R


It is possible upload a code to MSP432 using the UART interface and an external USB/serial converter (like as FTDI based, for example)? I want to produce a custom board for mass production but I would not like to embed a programmer like as the XDS110-ET in my board or use an external and expensive programmer. My requirements are restricted to upload the code for flash memory of MSP432. No debugging capability are required. I've been choosing the right microcontroller for my application and MSP432 is suitable for that. But I need ensure that MSP432 may be programmed using a simple UART connection.

**Attention** This is a public forum