Other Parts Discussed in Thread: ADS5560, DAC7760
I have a Launchxl-F28377S but it seems not suitable to my application and I wonder which microcontroller in low-power family is suitable to this application? It is not easier to figure out one in this family.
The application:
Impedance measurement
Input siganl: Sine wave 10MHz. The aquisition rate and SNR of the ADCs on the Launchpad can't fit this requirement therefore a ADC is reqired, such as ADS5560.
Output signal: 0-10V and +/-10V. The bipolar output DAC is required, for example, DAC7760.
PWM, encoders are not neccessary in this application.