Hi, is there a migration guide from F249 to F5528? Is there pin mux program available for 5528?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AFAIK, no. And IMHO it would make no sense. The 2x and 5x series have so many differences that a migration guide would be more complex than a 'howto 5528 from scratch'.Arrow Vancouver said:Hi, is there a migration guide from F249 to F5528?
There's no need to. Using the pin mux feature is 100% straight. Just a series of 'pin x = function y' instructions. Writing a program for that is plain overkill.Arrow Vancouver said:Is there pin mux program available for 5528
**Attention** This is a public forum