This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5972: UART

Part Number: MSP430FR5972


Hi,

I am using CCS v7, device MSP430FR5972. I am just trying to run UART. Just send anything from PC keyboard want to receive the same but not working.

my coding is below:

#include <msp430.h>

int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog

// Configure GPIO
P2SEL0 |= BIT0 | BIT1; // USCI_A0 UART operation
P2SEL1 &= ~(BIT0 | BIT1);

// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;

// Startup clock system with max DCO setting ~8MHz
CSCTL0_H = CSKEY >> 8; // Unlock clock registers
CSCTL1 = DCOFSEL_3 | DCORSEL; // Set DCO to 8MHz

CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL0_H = 0; // Lock CS registers

// Configure USCI_A0 for UART mode
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset

UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK

// Baud Rate calculation
// 8000000/(16*9600) = 52.083
// Fractional portion = 0.083
// User's Guide Table 21-4: UCBRSx = 0x04
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BR0 = 52; // 8000000/16/9600
UCA0BR1 = 0x00;
FRCTL0 = FRCTLPW | NWAITS_1; // Change the NACCESS_x value to add the right amount of waitstates

UCA0MCTLW |= UCOS16 | UCBRF_1 | 0x4900;
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt

__bis_SR_register(LPM3_bits | GIE); // Enter LPM3, interrupts enabled
__no_operation(); // For debugger
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:

while(!(UCA0IFG&UCTXIFG));

UCA0TXBUF = UCA0RXBUF;

__no_operation();
break;
case USCI_UART_UCTXIFG: break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
}
}

Also using USB-TTL device and connect Rx-Tx, Tx-Rx & GND common. Set baud rate 9600 on Hyper terminal. 

 

**Attention** This is a public forum