Part Number: MSP430F5529
Tool/software: TI C/C++ Compiler
Hello,
Please I am trying to measure the period of a signal with an MSP430F5529 launchpad. The signal is fed to the MCU via P1.2. I am using TA0 with the CCR1 register in capture mode. When debugging the program, the main application i.e. the LED blinking part of the code works, but immediately interrupts are enabled, the program below runs (isr_trap.asm). This causes the entire application to hang. Please I need help to fix this issue, thank you.
;****************************************************************************** ;* ISR_TRAP.ASM - v15.12.1 * ;* * ;* Copyright (c) 2003-2016 Texas Instruments Incorporated * ;* http://www.ti.com/ * ;* * ;* Redistribution and use in source and binary forms, with or without * ;* modification, are permitted provided that the following conditions * ;* are met: * ;* * ;* Redistributions of source code must retain the above copyright * ;* notice, this list of conditions and the following disclaimer. * ;* * ;* Redistributions in binary form must reproduce the above copyright * ;* notice, this list of conditions and the following disclaimer in * ;* the documentation and/or other materials provided with the * ;* distribution. * ;* * ;* Neither the name of Texas Instruments Incorporated nor the names * ;* of its contributors may be used to endorse or promote products * ;* derived from this software without specific prior written * ;* permission. * ;* * ;* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * ;* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * ;* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * ;* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * ;* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * ;* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * ;* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * ;* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * ;* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * ;* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * ;* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ;* * ;****************************************************************************** ;----------------------------------------------------------------------------- ;-- default ISR handler if user does not supply ;-- simply puts device into lpm0 ;----------------------------------------------------------------------------- .sect ".text:_isr:__TI_ISR_TRAP" .align 2 .global __TI_ISR_TRAP __TI_ISR_TRAP: BIS.W #(0x0010),SR JMP __TI_ISR_TRAP NOP ; CPU40 Compatibility NOP ;****************************************************************************** ;* BUILD ATTRIBUTES * ;* HW_MPY_INLINE_INFO=1: file does not have any inlined hw mpy * ;* HW_MPY_ISR_INFO =1: file does not have ISR's with mpy or func calls * ;****************************************************************************** .battr "TI", Tag_File, 1, Tag_HW_MPY_INLINE_INFO(1) .battr "TI", Tag_File, 1, Tag_HW_MPY_ISR_INFO(1)
Please this is the program I am debugging:
/**
* Section: Included Files
*/
#include <stdio.h>
#include <stdint.h>
#include "driverlib.h"
#include "LCD_driver.h"
/**
* Section: Global Variables Definitions
*/
uint16_t period_raw = 0;
uint16_t captured_value;
uint16_t previous_capture;
float period_old;
float period_new;
float period_change;
float calibrated_capacitance;
float measured_capacitance;
/**
* Section: Macro Declarations
*/
#define RA 1000 // value of resistor RA in ohms
#define RB 10000 // value of resistor RB in ohms
#define K (1.44 / ((RA) + (2 * RB))) // constant for determining the capacitance
#define P 1 // value of one timer tick in seconds (redefine this value)
/**
* Section: Function Prototypes
*/
void capture_config(void);
inline void capture_interrupt(void);
/**
* Section: Main Application
*/
int main(void)
{
WDT_A_hold(WDT_A_BASE); // Stop watchdog timer
GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
capture_config(); // configure timerA for capture mode
delay_ms(50); // allow 555 timer to stabilize?
char display_data[20];
while(1)
{
if(TIMER_A_CAPTURE_OVERFLOW == Timer_A_getCaptureCompareInterruptStatus\
(TIMER_A0_BASE, TIMER_A_CAPTURECOMPARE_REGISTER_1, TIMER_A_CAPTURE_OVERFLOW))
{
// reset timer?
}
//blink led
GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
delay_ms(1000);
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
delay_ms(1000);
}
}
/**
* Section: Function Definitions
*/
void capture_config(void)
{
// set P1.2 as input
GPIO_setAsInputPin(GPIO_PORT_P1, GPIO_PIN2);
// set P1.2 as capture input
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1, GPIO_PIN2);
// initialize timerA for continuous mode operation
Timer_A_initContinuousModeParam continuous_param = {0};
continuous_param.clockSource = TIMER_A_CLOCKSOURCE_SMCLK;
continuous_param.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
continuous_param.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE;
continuous_param.timerClear = TIMER_A_DO_CLEAR;
continuous_param.startTimer = false;
Timer_A_initContinuousMode(TIMER_A0_BASE, &continuous_param);
// initialize timerA capture mode
Timer_A_clearCaptureCompareInterrupt(TIMER_A0_BASE, TIMER_A_CAPTURECOMPARE_REGISTER_0);
Timer_A_initCaptureModeParam capture_param = {0};
capture_param.captureRegister = TIMER_A_CAPTURECOMPARE_REGISTER_1;
capture_param.captureInterruptEnable = TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE;
capture_param.captureMode = TIMER_A_CAPTUREMODE_RISING_EDGE;
capture_param.captureInputSelect = TIMER_A_CAPTURE_INPUTSELECT_CCIxA;
capture_param.synchronizeCaptureSource = TIMER_A_CAPTURE_SYNCHRONOUS;
capture_param.captureOutputMode = TIMER_A_OUTPUTMODE_OUTBITVALUE;
Timer_A_initCaptureMode(TIMER_A0_BASE, &capture_param);
Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_CONTINUOUS_MODE);
// enable interrupts
__bis_SR_register(GIE);
}
inline void capture_interrupt(void)
{
static uint8_t interrupt_number = 0;
interrupt_number++;
// get captured value
captured_value = Timer_A_getCaptureCompareCount(TIMER_A0_BASE, TIMER_A_CAPTURECOMPARE_REGISTER_1);
if(interrupt_number == 1)
{
previous_capture = captured_value;
}
if(interrupt_number == 2)
{
period_raw = captured_value - previous_capture;
interrupt_number = 0;
}
}
/**
* Section: Interrupt Service Routine
*/
#pragma vector=TIMER1_A1_VECTOR
__interrupt void TIMER_A0_ISR(void)
{
switch(__even_in_range(TA0IV, 14))
{
case 0: // none
break;
case 2: // CCR1 IFG
capture_interrupt();
break;
case 4: // CCR2 IFG
break;
case 6: // CCR3 IFG
break;
case 8: // CCR4 IFG
break;
case 10: // CCR5 IFG
break;
case 12: // CCR6 IFG
break;
case 14: // TAOIFG
break;
default: // never executed
break;
}
}
Although the application hangs, viewing the CCR1 register in the watches window confirmed that the capture mode of the timer was at work when fed with a 1KHz signal from a signal generator. A screenshot of this is shown below: