Part Number: MSP430F6659
Hello sir,
i want to use usb module of msp430f6659. i have downloaded MSP430USBDevelopersPackage_5_10_00_17 and installed MSPUSBDescriptorTool-5_00_10_19 as well as HID demo app.
i use H6_SendDataBackground example from above package. Using descriptor tool i generate code as per my setting and overwrite it to files in USB_Config folder.
I have made hardware as per slaa457a datasheet page no 14. In hardware i do not connect any external supply on VUSB pin as a want to use it from VBUS . I want to use separate power supply for microcontroller(other than USB module) which is external 3.3V supply and it remain on independent of weather usb connected with pc or not.
I want to use VBUS spply only for USB module.
my XT2 crystal is 16.384MHZ.
i have not made any other change in example.I want to use HID interface
when i connect this hardware to pc it shows UNKNOWN DEVICE.
please help me that how can i setup usb so it works properly.
it is required to configure clock and port pin separately or it is included in example ?
please mention the necessary changes that i have to do for make it working.