This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
Is it possible to periodically trigger the ADC to sample in autoscan mode? I would like the set up the adc to read an array of sensor periodically but not continuously. I've tried to combined driver library examples
"adc14_multiple_channel_no_repeat" and "adc14_single_conversion_repeat_timera_source", using the parts from both that i thought would work. The code I have now does a conversion for the sequence only
once and never enters the ISR again. My project will required the sensor array to be sample at a rate of 15 - 25 Hz.
I would appreciate if someone could review my code and give me some insight.
/* * ------------------------------------------- * MSP432 DriverLib - v3_21_00_05 * ------------------------------------------- * * --COPYRIGHT--,BSD,BSD * Copyright (c) 2016, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ /******************************************************************************* * MSP432 ADC14 - Multiple Channel Sample without Repeat * * Description: In this code example, the feature of being able to scan multiple * ADC channels is demonstrated by the user a the DriverLib APIs. Conversion * memory registers ADC_MEM0 - ADC_MEM7 are configured to read conversion * results from A0-A7 respectively. Conversion is enabled and then sampling is * toggled using a software toggle. Repeat mode is not enabled and sampling only * occurs once (and it is expected that the user pauses the debugger to observe * the results). Once the final sample has been taken, the interrupt for * ADC_MEM7 is triggered and the result is stored in the resultsBuffer buffer. * * MSP432P401 * ------------------ * /|\| | * | | | * --|RST P5.5 |<--- A0 (Analog Input) * | P5.4 |<--- A1 (Analog Input) * | P5.3 |<--- A2 (Analog Input) * | P5.2 |<--- A3 (Analog Input) * | P5.1 |<--- A4 (Analog Input) * | P5.0 |<--- A5 (Analog Input) * | P4.7 |<--- A6 (Analog Input) * | P4.6 |<--- A7 (Analog Input) * | | * | | * * Author: Timothy Logan ******************************************************************************/ /* DriverLib Includes */ #include "driverlib.h" /* Standard Includes */ #include <stdint.h> #include <stdbool.h> #include <string.h> static uint16_t resultsBuffer[8]; /* Timer_A Continuous Mode Configuration Parameter */ const Timer_A_UpModeConfig upModeConfig = { TIMER_A_CLOCKSOURCE_ACLK, // ACLK Clock Source TIMER_A_CLOCKSOURCE_DIVIDER_1, // ACLK/1 = 32Khz 16384, TIMER_A_TAIE_INTERRUPT_DISABLE, // Disable Timer ISR TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE, // Disable CCR0 TIMER_A_DO_CLEAR // Clear Counter }; /* Timer_A Compare Configuration Parameter */ const Timer_A_CompareModeConfig compareConfig = { TIMER_A_CAPTURECOMPARE_REGISTER_1, // Use CCR1 TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE, // Disable CCR interrupt TIMER_A_OUTPUTMODE_SET_RESET, // Toggle output but 16384 // 16000 Period }; int main(void) { /* Halting WDT */ MAP_WDT_A_holdTimer(); MAP_Interrupt_enableSleepOnIsrExit(); /* Zero-filling buffer */ memset(resultsBuffer, 0x00, 8); /* Setting up clocks * MCLK = MCLK = 3MHz * ACLK = REFO = 32Khz */ MAP_CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1); /* Setting reference voltage to 2.5 and enabling reference */ MAP_REF_A_setReferenceVoltage(REF_A_VREF2_5V); MAP_REF_A_enableReferenceVoltage(); /* Initializing ADC (MCLK/1/1) */ MAP_ADC14_enableModule(); MAP_ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1, 0); /* Configuring GPIOs for Analog In */ MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5, GPIO_PIN5 | GPIO_PIN4 | GPIO_PIN3 | GPIO_PIN2 | GPIO_PIN1 | GPIO_PIN0, GPIO_TERTIARY_MODULE_FUNCTION); MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P4, GPIO_PIN7 | GPIO_PIN6, GPIO_TERTIARY_MODULE_FUNCTION); /* Configuring ADC Memory (ADC_MEM0 - ADC_MEM7 (A0 - A7) with no repeat) * with internal 2.5v reference */ MAP_ADC14_configureMultiSequenceMode(ADC_MEM0, ADC_MEM7, false); MAP_ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A0, false); MAP_ADC14_configureConversionMemory(ADC_MEM1, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A1, false); MAP_ADC14_configureConversionMemory(ADC_MEM2, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A2, false); MAP_ADC14_configureConversionMemory(ADC_MEM3, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A3, false); MAP_ADC14_configureConversionMemory(ADC_MEM4, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A4, false); MAP_ADC14_configureConversionMemory(ADC_MEM5, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A5, false); MAP_ADC14_configureConversionMemory(ADC_MEM6, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A6, false); MAP_ADC14_configureConversionMemory(ADC_MEM7, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A7, false); //----------------------------------------------------------- /* Configuring Timer_A in continuous mode and sourced from ACLK */ MAP_Timer_A_configureUpMode(TIMER_A0_BASE, &upModeConfig); /* Configuring Timer_A0 in CCR1 to trigger at 16000 (0.5s) */ MAP_Timer_A_initCompare(TIMER_A0_BASE, &compareConfig); /* Configuring the sample trigger to be sourced from Timer_A0 and setting it * to automatic iteration after it is triggered*/ MAP_ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false); MAP_ADC14_enableSampleTimer(ADC_MANUAL_ITERATION); /* Enabling the interrupt when a conversion on channel 7 (end of sequence) * is complete and enabling conversions */ MAP_ADC14_enableInterrupt(ADC_INT7); MAP_ADC14_enableConversion(); /* Enabling Interrupts */ MAP_Interrupt_enableInterrupt(INT_ADC14); MAP_Interrupt_enableMaster(); /* Starting the Timer */ MAP_Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_UP_MODE); /* Going to sleep */ while (1) { MAP_PCM_gotoLPM0(); } } /* This interrupt is fired whenever a conversion is completed and placed in * ADC_MEM7. This signals the end of conversion and the results array is * grabbed and placed in resultsBuffer */ void ADC14_IRQHandler(void) { uint64_t status; status = MAP_ADC14_getEnabledInterruptStatus(); MAP_ADC14_clearInterruptFlag(status); if(status & ADC_INT7) { MAP_ADC14_getMultiSequenceResult(resultsBuffer); } }
Andre,
In order to repeat the sequence of channels on the next timer trigger you would need to clear and then reset the ADC14ENC bit. I have attached two examples and the no-repeat example shows how the 6Hz is used to trigger each sequence of channels, while the repeat shows how the 6Hz is used continuously trigger each channel within the sequence of channels - so the effective sampling rate is 2hz (measuring 3 channels).
Hope this helps,
Chris
/* * adc14_multiple_channel_no_repeat_timera_source_01.c * * Timer (2hz) Triggered sequence of conversions (ADC14 6,7,8), * where each conversion in the sequence is performed immediately * after the previous. After the last conversion in the sequence * the ADC14 waits for the timer trigger. * The ISR moves information from ADCMEM6-ADCMEME8 to three * seperate buffers buffer0[64], buffer1[64], buffer2[64] * */ #include "driverlib.h" /* Standard Includes */ #include <stdint.h> #include <string.h> #define NUMBER_OF_SAMPLES 64 uint32_t prim_buffer0[NUMBER_OF_SAMPLES]; uint32_t prim_buffer1[NUMBER_OF_SAMPLES]; uint32_t prim_buffer2[NUMBER_OF_SAMPLES]; /* Timer_A Continuous Mode Configuration Parameter */ const Timer_A_UpModeConfig upModeConfig = { TIMER_A_CLOCKSOURCE_SMCLK, // SMCLK Clock Source TIMER_A_CLOCKSOURCE_DIVIDER_8, // SMCLK/8 = 125khz 62500, // 0.5 seconds -> 2Hz TIMER_A_TAIE_INTERRUPT_DISABLE, // Disable Timer ISR TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE, // Disable CCR0 TIMER_A_DO_CLEAR // Clear Counter }; /* Timer_A Compare Configuration Parameter */ const Timer_A_CompareModeConfig compareConfig = { TIMER_A_CAPTURECOMPARE_REGISTER_1, // Use CCR1 TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE, // Disable CCR interrupt TIMER_A_OUTPUTMODE_SET_RESET, // Toggle output but 62500 // }; uint16_t measureIndex; int main(void) { /* Halting WDT */ MAP_WDT_A_holdTimer(); MAP_Interrupt_disableMaster(); // MAP_Interrupt_enableSleepOnIsrExit(); SCB->SCR |= SCB_SCR_SLEEPDEEP_Pos; /* Zero-filling buffer */ memset(prim_buffer0,0x0000,NUMBER_OF_SAMPLES); memset(prim_buffer1,0x0000,NUMBER_OF_SAMPLES); memset(prim_buffer2,0x0000,NUMBER_OF_SAMPLES); measureIndex = 0; /* * Configure DCO for 8Mhz operation */ /* Enabling FPU for DCO Frequency calculation */ MAP_FPU_enableModule(); /* Setting the DCO Frequency to a 8MHz */ MAP_CS_setDCOFrequency(8000000); /* * Setting up clocks * SMCLK = DCO/8 = 1MHz */ MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1); MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_8); /* Setting reference voltage to 2.5 and enabling reference */ MAP_REF_A_setReferenceVoltage(REF_A_VREF2_5V); MAP_REF_A_enableReferenceVoltage(); /* Initializing ADC (MCLK/1/1) */ MAP_ADC14_enableModule(); MAP_ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1, 0); /* Configuring GPIOs for Analog In P4.5,4.6,4.7 */ MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P4, GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_TERTIARY_MODULE_FUNCTION); /* Configuring P1.0 as output */ MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); /* Configuring ADC Memory (ADC_MEM6 - ADC_MEM8 (A6 - A8) without repeat) * with internal 2.5v reference */ MAP_ADC14_configureMultiSequenceMode(ADC_MEM6, ADC_MEM8, false); MAP_ADC14_configureConversionMemory(ADC_MEM6, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A6, false); MAP_ADC14_configureConversionMemory(ADC_MEM7, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A7, false); MAP_ADC14_configureConversionMemory(ADC_MEM8, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A8, false); /* Configuring Timer_A in continuous mode and sourced from SMCLK */ MAP_Timer_A_configureUpMode(TIMER_A0_BASE, &upModeConfig); /* Configuring Timer_A0 in CCR1 to trigger at 0.5sec */ MAP_Timer_A_initCompare(TIMER_A0_BASE, &compareConfig); /* * Configuring the sample trigger to be sourced from Timer_A0 CCR1 * and setting it to automatic iteration after it is triggered */ MAP_ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false); /* * Setting up the sample timer to automatically step through the sequence * convert. */ MAP_ADC14_enableSampleTimer(ADC_AUTOMATIC_ITERATION); /* * Enabling the interrupt when a conversion on channel 8 * and enabling conversions */ MAP_ADC14_enableInterrupt(ADC_INT8); MAP_ADC14_enableConversion(); /* * Clear IFGs before enabling interrupt */ MAP_ADC14_clearInterruptFlag(0xFFFFFFFFFFFFFFFF); MAP_Interrupt_enableInterrupt(INT_ADC14); MAP_Interrupt_enableMaster(); /* Starting the Timer */ MAP_Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_UP_MODE); MAP_PCM_gotoLPM0(); __no_operation(); while(1); /* * Process three arrays */ } /* * This interrupt is fired whenever the sequence is completed * */ void ADC14_IRQHandler(void) { uint64_t status; // Turn on LED MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0); status = ADC14_getEnabledInterruptStatus(); MAP_ADC14_clearInterruptFlag(status); if(status & ADC_INT8) { MAP_ADC14_disableConversion(); prim_buffer0[measureIndex] = MAP_ADC14_getResult(ADC_MEM6); // Move A0 results, IFG is cleared prim_buffer1[measureIndex] = MAP_ADC14_getResult(ADC_MEM7); // Move A1 results, IFG is cleared prim_buffer2[measureIndex] = MAP_ADC14_getResult(ADC_MEM8); // Move A2 results, IFG is cleared // MAP_DMA_requestSoftwareTransfer(0); measureIndex++; __no_operation(); if(measureIndex == NUMBER_OF_SAMPLES) { /* * Stop Timer */ MAP_Timer_A_stopTimer(TIMER_A0_BASE); measureIndex = 0; //MAP_Interrupt_disableSleepOnIsrExit(); SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Pos; MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0); } else { MAP_ADC14_enableConversion(); } } }
/* * adc14_multiple_channel_repeat_timera_source_01.c * * Timer (6hz) Triggered sequence of conversions (ADC14 6,7,8), * where each conversion is triggered by the 6Hz timer. The * resulting sample rate of each channel is 2Hz - 3 intervals of * the 6Hz timer. * ISR moves information from ADCMEM6-ADCMEME8 to three seperate * buffers buffer0[64], buffer1[64], buffer2[64] * */ #include "driverlib.h" /* Standard Includes */ #include <stdint.h> #include <string.h> #define NUMBER_OF_SAMPLES 64 uint32_t prim_buffer0[NUMBER_OF_SAMPLES]; uint32_t prim_buffer1[NUMBER_OF_SAMPLES]; uint32_t prim_buffer2[NUMBER_OF_SAMPLES]; /* Timer_A Continuous Mode Configuration Parameter */ const Timer_A_UpModeConfig upModeConfig = { TIMER_A_CLOCKSOURCE_SMCLK, // SMCLK Clock Source TIMER_A_CLOCKSOURCE_DIVIDER_8, // SMCLK/8 = 125khz 20833, // 0.167 seconds -> 6Hz TIMER_A_TAIE_INTERRUPT_DISABLE, // Disable Timer ISR TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE, // Disable CCR0 TIMER_A_DO_CLEAR // Clear Counter }; /* Timer_A Compare Configuration Parameter */ const Timer_A_CompareModeConfig compareConfig = { TIMER_A_CAPTURECOMPARE_REGISTER_1, // Use CCR1 TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE, // Disable CCR interrupt TIMER_A_OUTPUTMODE_SET_RESET, // Toggle output but 20833 // }; uint16_t measureIndex; int main(void) { /* Halting WDT */ MAP_WDT_A_holdTimer(); MAP_Interrupt_disableMaster(); // MAP_Interrupt_enableSleepOnIsrExit(); SCB->SCR |= SCB_SCR_SLEEPDEEP_Pos; /* Zero-filling buffer */ memset(prim_buffer0,0x0000,NUMBER_OF_SAMPLES); memset(prim_buffer1,0x0000,NUMBER_OF_SAMPLES); memset(prim_buffer2,0x0000,NUMBER_OF_SAMPLES); measureIndex = 0; /* * Configure DCO for 8Mhz operation */ /* Enabling FPU for DCO Frequency calculation */ MAP_FPU_enableModule(); /* Setting the DCO Frequency to a 8MHz */ MAP_CS_setDCOFrequency(8000000); /* * Setting up clocks * SMCLK = DCO/8 = 1MHz */ MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1); MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_8); /* Setting reference voltage to 2.5 and enabling reference */ MAP_REF_A_setReferenceVoltage(REF_A_VREF2_5V); MAP_REF_A_enableReferenceVoltage(); /* Initializing ADC (MCLK/1/1) */ MAP_ADC14_enableModule(); MAP_ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1, 0); /* Configuring GPIOs for Analog In P4.5,4.6,4.7 */ MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P4, GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_TERTIARY_MODULE_FUNCTION); /* Configuring P1.0 as output */ MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); /* Configuring ADC Memory (ADC_MEM6 - ADC_MEM8 (A6 - A8) with repeat) * with internal 2.5v reference */ MAP_ADC14_configureMultiSequenceMode(ADC_MEM6, ADC_MEM8, true); MAP_ADC14_configureConversionMemory(ADC_MEM6, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A6, false); MAP_ADC14_configureConversionMemory(ADC_MEM7, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A7, false); MAP_ADC14_configureConversionMemory(ADC_MEM8, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A8, false); /* Configuring Timer_A in continuous mode and sourced from SMCLK */ MAP_Timer_A_configureUpMode(TIMER_A0_BASE, &upModeConfig); /* Configuring Timer_A0 in CCR1 to trigger at 0.5sec */ MAP_Timer_A_initCompare(TIMER_A0_BASE, &compareConfig); /* * Configuring the sample trigger to be sourced from Timer_A0 CCR1 * and setting it to automatic iteration after it is triggered */ MAP_ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false); /* * Setting up the sample timer to manually step through the sequence * convert. */ MAP_ADC14_enableSampleTimer(ADC_MANUAL_ITERATION); /* * Enabling the interrupt when a conversion on channel 8 * and enabling conversions */ MAP_ADC14_enableInterrupt(ADC_INT8); MAP_ADC14_enableConversion(); /* * Clear IFGs before enabling interrupt */ MAP_ADC14_clearInterruptFlag(0xFFFFFFFFFFFFFFFF); MAP_Interrupt_enableInterrupt(INT_ADC14); MAP_Interrupt_enableMaster(); /* Starting the Timer */ MAP_Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_UP_MODE); MAP_PCM_gotoLPM0(); __no_operation(); while(1); /* * Process three arrays */ } /* * This interrupt is fired whenever the sequence is completed * */ void ADC14_IRQHandler(void) { uint64_t status; // Turn on LED MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0); status = ADC14_getEnabledInterruptStatus(); MAP_ADC14_clearInterruptFlag(status); if(status & ADC_INT8) { prim_buffer0[measureIndex] = MAP_ADC14_getResult(ADC_MEM6); // Move A0 results, IFG is cleared prim_buffer1[measureIndex] = MAP_ADC14_getResult(ADC_MEM7); // Move A1 results, IFG is cleared prim_buffer2[measureIndex] = MAP_ADC14_getResult(ADC_MEM8); // Move A2 results, IFG is cleared measureIndex++; __no_operation(); if(measureIndex == NUMBER_OF_SAMPLES) { /* * Stop Timer */ MAP_Timer_A_stopTimer(TIMER_A0_BASE); measureIndex = 0; //MAP_Interrupt_disableSleepOnIsrExit(); SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Pos; MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0); } } }
**Attention** This is a public forum