Part Number: MSP430G2755
Hi all,
I am trying to configure a MSP430G2755 master to communicate with multiple MSP430G2755 slaves. I cannot use 4-pin mode because of the hardware wiring. What I am trying to do is related to this post: https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/302862
At the bottom of that post, it is mentioned a single master/multiple slave configuration can be achieved with 3 pin mode and I am hoping someone can provide more detail on how this can be accomplished. I have attempted initializing the spi state machine at start up but I seem to be getting some cross talk on the spi bus from slaves a,b,c when I am trying to talk to slave d for example. I also thought to initialize the slave spi state machine when the slave select is pulled low in a ISR, but my slave select pins are on P4 and not interruptible.
Does anyone have any other ideas?