Hello team,
Hope you are well.
Please see below question from the customer:
- I have looked at SLAU378 section 24.11.3.4, is there another location where I can find more information on how to select the trimmer capacitors? And is there a way to adjust the tuning of the antennas without using an external RF source?
- Is there a place where I can find code examples of using the LF receiver?
- Is there a way to have a transmitter that connects to the LF receiver using RF and a bit banging technique? And if so is there a place where I can find code examples of this? (Our system also uses beacons that we would like to use this part in, we need to precisely control the maximum beacon – badge range, within a few inches)
Regards,