Other Parts Discussed in Thread: MSP430F5528, MSPDS
I have two brand new Launchpad MSP430FR5969 boards that work like a champ on my Windows 7(64-bit) Desktop.
The desktop has CCS Version 7 installed.
I assume the install of CCS may have installed a USB-to-UART Driver?????
But...when I attach the LaunchPad to my 8-inch Windows 10(32 bit) Tablet...the Tablet and Launchpad never connect.
Device Manager on the Tablet shows no additional COM ports appearing.
Windows 10 gives no indication that it sees a newly plugged-in device attempting to attach.
Nor does Windows try to search the web to find the proper device driver.
USB cables are not the issue. The two cables I'm using for the Launchpad(Micro-USB) work fine attaching a Teensy Board(Micro-USB) to the Windows Tablet(Micro-USB).
My guess is that I need a device driver (or appropriate .inf file).
Installing CCS on the tablet is not an option...my 32MB disk already overloaded.
Ok, new information...the chip on this Launchpad that has the USB capability is the MSP430F5528 chip.
I wonder if the correct CDC device driver comes bundled with Windows 10...or maybe not. It would be nice if there was a stand alone .exe file to install the proper drivers on my Windows 10 tablet. Hopefully these Launchpad boards can be loaded with user code, and connected to different Windows desktops PC, laptops, or tablets... without having to load the full blown CCS development system on each sysem.