Hi everyone,
Sorryme for the noobish question but I can't seem to find an answer anywhere. Is the 868mhz Chronos watch able to transmit to the lower frequencies? I want to use it to open my car barrier which uses 433mhz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
Sorryme for the noobish question but I can't seem to find an answer anywhere. Is the 868mhz Chronos watch able to transmit to the lower frequencies? I want to use it to open my car barrier which uses 433mhz.
Hi Kostadin,
Unfortunately the antenna provided on the eZ430-Chronos-868 is not matched for other frequencies and is therefore incompatible with the 433-MHz band. There are also software differences between the two solutions that will impede you from frequency hopping capabilities. You are most likely aware that the eZ430-Chronos-433 is obsolete so your options in this regard are limited. All of this information is covered on the EZ430-CHRONOS tool and Wiki pages.
Regards,
Ryan
**Attention** This is a public forum