Part Number: SIMPLELINK-MSP432-SDK
Tool/software: Starterware
Hi,
Now I am using the MSP432 launchpad. But I find it difficult to start with the demo in simplelink SDK while using rtos. I mean the examples provided is too simple to use. For example there is no uart demo combined with DMA. When dubugging interrupts, I can find msp432_startup_ccs.c no where, which is included in project files in no rtos condition. How to achieve my interrupt with rtos?
I am confused that the SDK well supports the development of MSP432 using no rtos, but not very friendly to rtos customers. Since MSP432 is based on M4 core, I think abstract api drivers should be supported better like STM32 series.
Are there any documents explain my confuse? I need help.
Than you!