This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer_A: TACLR and MCx

Other Parts Discussed in Thread: MSP430F2132

Hi there

I'm using a MSP430F2132. Just now I noticed, that setting the TACLR bit in the TA0CTL register doesn't reset the count direction defined by the MCx bits, which is contrary to the description of the TACLR bit in the user's guide. However, the block diagram of the Timer_A shows no connection between TACLR and the Count Mode block. Thus, I guess the behaviour of the MSP430 ist correct and the description of the TACLR bit is incorrect. Is this right?

Regards

Roman

**Attention** This is a public forum