Other Parts Discussed in Thread: ENERGIA
Hi guys
I'm trying to record sound with a msp432 board and I want to change the sample rate of its ADC, but when I looked at the example of standard Energia code AnalogRead(), there is a line of statement said" It takes about 100 microseconds (0.0001 s) to read an analog input, so the maximum reading rate is about 10,000 times a second." does it mean that this code has already set the sample rate of ADC in 10KHZ and there is no way I can change it?
If I want to change the sample rate of ADC, how can I do it?
Thanks a lot
Barry