This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: Setting up ADC14

Part Number: MSP432P401R


Tool/software: Code Composer Studio

Hello,

I am using my MSP432P401R board and i am trying to setup a simple program that for single channel and single conversion and display it on to a Nokia 5110 LCD (red). A potentiometer is attached is attached to PIN 5.1 for ADC, however i am not able to get this program working, if anyone can please point out what i am missing for this program. Just for your information, i am new to the MSP Microcontroller

#include <stdint.h>
#include "Nokia5110.c"
#include "ClockSystem.c"
#include "msp432.h"
#include "msp432p401r.h"
void ADC_setup(void);


int main(void)
{

WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
__enable_interrupt(); //enable global interrupt
// P5->REN|=BIT1; //set REN bit on port 1 as 1
// P5->OUT|=BIT1; // set OUT bit on port 1 as 1
Nokia5110_Init(); // initialize LCD
uint32_t value;
ADC_setup();

// Nokia5110_Clear();//Clear screen


while(1)
{
ADC14->CTL0|=ADC14_CTL0_SC;//Start Conversion
// Delay(5000);
value=ADC14->MEM[13];
Nokia5110_Clear();//Clear screen
Nokia5110_SetCursor(4, 2); // Display on Row 4, Column 1 of LCD
Nokia5110_OutUDec(value);

}

}

void ADC_setup(void){
CS->KEY |= 0x00001111;//Unlock All Registers for Clock
CS->CTL1|=CS_CTL1_DIVM_1;
//Set Pin on 5_1 of Pin Map as input
P5->SEL0 |= (BIT1); // SEL0 and SEL1 are set to 1 to enable Analog A4
P5->SEL1 |= (BIT1);
P5->DIR &= ~(BIT1);// The pin is set as input

ADC14->CTL0|=ADC14_CTL0_ON;//Turn on ADC Core
ADC14->CTL0|=ADC14_CTL0_CONSEQ_0;//Using Mode Single Channel Single Conversion
ADC14->CTL1|=ADC14_CTL1_RES_1;// Conversion result resolution of 12-bit
ADC14->MCTL[13]|=ADC14_MCTLN_INCH_4;
ADC14->CTL0&=~(ADC14_CTL0_SSEL_0);
ADC14->CTL1|=0X0D0000;
ADC14->CTL0|= ADC14_CTL0_SSEL_3;
ADC14->CTL0|= ADC14_CTL0_DIV_1;
ADC14->CTL0|=ADC14_CTL0_ENC;//Enable Conversion


}

**Attention** This is a public forum