1) Is there going to be a separate forum for just the LaunchPad? Given its popularity, I predict that that might be a good idea. There are sure to be a large number of "beginner issues" that it might make sense to segregate as much as possible (even if that is a politically incorrect word.) I've noticed that a large portion of beginner questions can actually be helpful to establishing a community (the beginners help each other, and often come up with questions that make even the experiences users think), but that doesn't mean that everyone in THIS forum will be happy with the traffic level...
2) Given that digital IO ports on MSP430x2xx have configurable internal pullup/pulldown resistors, why is there an EXTERNAL pullup the p1.3 pin of the launchpad design? Compatibility with 1xx series chips?