Hi,
I am using MSP430F5529 on my board. I require MSP to remember some passcodes (4 digit numbers) when it goes to sleep mode to save power (currently LPM3). Is MSP capable of saving those passcodes in the internal flash? Can the internal flash be used for storing miscellaneous data or it is just used to save the main code binary? what about RAM, can I save the passcodes in the RAM and preserve it when the device goes to LPM3?
Thanks,
Danial