This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432-DEBUGGERS: MSP-TS432PZ100 Socket board BSL Header design

Part Number: MSP432-DEBUGGERS
Other Parts Discussed in Thread: MSP-FET

hi,

I saw the BSL HEADER on the MSP-TS432PZ100, it includes pins of  BSL_TX, BSL_RX, RSTN, BSL 9 and BSL 10

especially the BSL 9 and 10, using the JP3, JP4,JP5 to select using UART or I2C or SPI,

1. is it really support SPI when  use the MSP-FET?

2. is there any HW invoke GPIO for BSL entry?

**Attention** This is a public forum