Part Number: MSP430F5247
Hi,
in MSP430F5/6's UG(slau208), there has tables describe about the timing error rate in different UART setting,
but it lacks data of 25MHz, do you know what's tha value in red square below?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5247
Hi,
in MSP430F5/6's UG(slau208), there has tables describe about the timing error rate in different UART setting,
but it lacks data of 25MHz, do you know what's tha value in red square below?
See the USCI UART Calculator (which recommends BRS = 0):
Max. TX bit error: -0.07039999999958191(-0.07039999999958191, 0)
Max. RX bit error (sync.: -0.5 BRCLK): -0.22079999999972955(-0.22079999999972955,0)
Max. RX bit error (sync.: +/-0 BRCLK): -0.1439999999997693(-0.1439999999997693,0)
Max. RX bit error (sync.: +0.5 BRCLK): -0.06719999999980908(-0.06719999999980908,0)
Max. RX bit error (over: -0.5,0,+0.5): 0(-0.22079999999972955,0)
**Attention** This is a public forum