This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I am trying assembly language programming in msp430g2553. The code is given below:-
.cdecls C,LIST,"msp430g2231.h"
RESET mov.w #0280h,SP
StopWDT mov.w #WDTPW+WDTHOLD,&WDTCTL
SetupP1 mov.b #001h,&P1DIR
mov.b #000h,&P1OUT
bis.b #008h,&P1REN
bis.b #008h,&P1IE
bis.b #008h,&P1IES
bis.b #008h,&P1IFG
Mainloop bis.w #GIE,SR
nop
P1_ISR;
xor.b #001h,&P1OUT
bic.b #008h,&P1IFG
reti
.sect ".reset"
.short RESET
.sect ".int02"
.short P1_ISR
.end
But I am getting a problem always in the Console Window which is as under:-
**** Build of configuration Debug for project weropisf ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../led.asm'
'Invoking: MSP430 Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/bin/cl430" -vmsp --abi=eabi --data_model=small --code_model=small --use_hw_mpy=none --include_path="C:/ti/ccsv6/ccs_base/msp430/include" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/include" --advice:power=all -g --define=__MSP430G2553__ --diag_warning=225 --diag_wrap=off --display_error_number --printf_support=minimal --preproc_with_compile --preproc_dependency="led.pp" "../led.asm"
'Finished building: ../led.asm'
' '
'Building target: weropisf.out'
'Invoking: MSP430 Linker'
"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/bin/cl430" -vmsp --abi=eabi --data_model=small --code_model=small --use_hw_mpy=none --advice:power=all -g --define=__MSP430G2553__ --diag_warning=225 --diag_wrap=off --display_error_number --printf_support=minimal -z -m"weropisf.map" --heap_size=0 --stack_size=0 -i"C:/ti/ccsv6/ccs_base/msp430/include" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="weropisf_linkInfo.xml" --use_hw_mpy=none --entry_point=RESET -o "weropisf.out" "./led.obj" "../lnk_msp430g2553.cmd" -l"rts430.lib"
<Linking>
fatal error #16000: object files have incompatible formats ("C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/lib/rts430.lib<int00.obj>" = TI-COFF, "./led.obj" = ELF)
>> Compilation failure
gmake: *** [weropisf.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Please help me in resolving this.
I had no issues with the following, CCS v6.2 and TI v16.9.2.LTS. Make sure that you are using eabi (ELF) output format under Project Properties -> General.
;------------------------------------------------------------------------------- .cdecls C,LIST,"msp430g2553.h" ; Include device header file ;------------------------------------------------------------------------------- .def RESET ; Export program entry-point to ; make it known to linker. ;------------------------------------------------------------------------------- .text ; Assemble into program memory. .retain ; Override ELF conditional linking ; and retain current section. .retainrefs ; And retain any sections that have ; references to current section. ;------------------------------------------------------------------------------- RESET mov.w #__STACK_END,SP ; Initialize stackpointer StopWDT mov.w #WDTPW|WDTHOLD,&WDTCTL ; Stop watchdog timer ;------------------------------------------------------------------------------- ; Main loop here ;------------------------------------------------------------------------------- mov.b #000h,&P1OUT bis.b #008h,&P1REN bis.b #008h,&P1IE bis.b #008h,&P1IES bis.b #008h,&P1IFG Mainloop bis.w #GIE,SR nop P1_ISR; xor.b #001h,&P1OUT bic.b #008h,&P1IFG reti ;------------------------------------------------------------------------------- ; Stack Pointer definition ;------------------------------------------------------------------------------- .global __STACK_END .sect .stack ;------------------------------------------------------------------------------- ; Interrupt Vectors ;------------------------------------------------------------------------------- .sect ".reset" ; MSP430 RESET Vector .short RESET .sect ".int02" .short P1_ISR .end
Regards, Ryan
**Attention** This is a public forum