This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969: Minor documentation error

Part Number: MSP430FR5969

On page 661 of  "SLAU367M–October 2012–Revised January 2017", bit 12 of UCBxIFG (UCRXIFG3) is incorrectly described as :

"Receive interrupt flag 2. UCRXIFG2 is set when UCBxRXBUF has received a
complete byte in slave mode and if the slave address defined in UCBxI2COA2
was on the bus in the same frame."

The curse of cut-n-paste!

Minor, but, hey...

**Attention** This is a public forum