Hey, I have an example code from Resource Explorer where it reads the ADC value on 2 pins. Pins 1.0,1.1 and stores the ADC values in ADC_Result Array. If i plug all 2 ports into 3.3V i get 255 which is the 8 bit conversion result for 3.3 V but I want the 10 bit result. How do I change it?
#include <msp430.h>
unsigned char ADC_Result[2]; // 8-bit ADC conversion result array
unsigned char i;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure ADC A0~2 pins
P1SEL0 |= BIT0 + BIT1;
P1SEL1 |= BIT0 + BIT1;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC
ADCCTL0 |= ADCSHT_2 | ADCMSC | ADCON; // 16ADCclks, MSC, ADC ON
ADCCTL1 |= ADCSHP | ADCCONSEQ_1 | ADCSSEL_1; // ADC clock ACLK, sampling timer, s/w trig.,single sequence
ADCCTL2 |= ADCRES_1; //10-bit conversion results
ADCMCTL0 |= ADCINCH_1 | ADCSREF_1; // A0~2(EoS); Vref=1.5V
ADCIE |= ADCIE0; // Enable ADC conv complete interrupt
// Configure reference
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
__delay_cycles(400); // Delay for reference settling
__no_operation();
while(1)
{
i = 1;
while(ADCCTL1 & ADCBUSY); // Wait if ADC core is active
ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/ interrupts
__no_operation(); // Only for debug
__delay_cycles(5000);
__no_operation();
}
}
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
ADC_Result[i] = ADCMEM0;
if(i == 0)
{
__bic_SR_register_on_exit(LPM0_bits); // Exist LPM0
}
else
{
i--;
}
break;
default:
break;
}
}