Other Parts Discussed in Thread: MAX3221E
Hello Everyone,
I am working on my own MSP432P401M controller. I have interface MSP432 MCU with MAX3221E IC. Microcontroller is transmitting the data. I have confirmed that on DSO. But, the level convertor IC is not operating properly (not giving output).Surprisingly,I have also observe that i am able to receive the externally send data ( MAX322 IC is receiving the data but not transmitting).I am attaching the screenshot of the circuit diagram.
Please comment on exactly where FORCEON and FORCEOFF connection and confirm our connection is right or not?? If the connections are wrong and If this is the case that i am not able to transmit the data. So, what are the proper connections of FORCEON and FORCEOFF pin . Currently I am not connecting TVS824022 TVS diode and C11,C12 capacitor. So, they are not causing any issue??
Thanks