Part Number: EZ430-F2013
I am trying to work out what the actual point of the eZ430-F2013 dongle is.
I can understand the whole USB debugger + detachable target board thing, but this design seems pretty pointless to me (and yes, I do own one, but have never found a use for it).
The fact that the whole thing is encased in a plastic case that you can't open easily (needs a spudger to lever it open) means that you can't use it as a programmer for a board you want to detach and use elsewhere - you may as well just throw the case away.
There's not much point in the detachable board since you only have one. I estimate the cost of the detachable board is probably about 0.1% of the entire device.
If the case only covered the debugger with a socket protruding out of it to plug target boards into I could understand it. And if you were provided with (or could buy) multiple target boards for it I could understand it. If the target board connector were of a standard 0.1" pitch so you could use standard "dupont" style jumper cables to program other boards I could understand it.
As it is it seems like it's a case of "Oh, we have these spare cases. Let's make a development board to fit it".
So has anyone actually used these things for a real project?