Hi,
I have a custom board built and have been having problems programming the MSP430F5419 in SBW mode.
I currently get the message: "MSP430: Error connecting to the target: No MSP430 device was found on USB FET 1".
I have setup my board as suggested in the slau278e app note. I have one board with 1nf and one with nothing for C1. The MSP430 are powered through the board and not the tool.
When I first built the boards they would program fine. Then they started having issues where I would have to cycle the power to program them. Until they eventually stopped working completely. What could possibly cause this degradation to happen?
BTW, the programmer is working fine with the evaluation board and the same chip with the jumpers matching my configuration.
Any suggestions?
Thanks,
Dan