This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am not able to simply open the out of box experience for CCS for MSP-EXP430FR5994.
I have made attempts using CCS's 'TI Resource Explorer' to select Example 'Out of Box Experience'
I have also tried using the TI Resource explorer to load individually provided Code examples.
The failure consists of clicking on Step 1: Import the example project into CCS.
At which point a small window pops up and disappears before displaying any information in addition to not loading the example into the Project Explorer.
I have made a parrallel attempt by downloading and loading the project without the TI Resource Explorer.
MSP-EXP430FR5994_Software_Examples_windows
from
software-dl.ti.com/.../index_FDS.html
This attempt fails the same way.
I have made a few attempts at loading other projects from TI Resource Explorer.
I have success in attempting Out Of Box examples for:
MSP-EXP430G2,
MSP-EXP430F5529LP,
MSP-EXP430FR5969,
MSP-EXP430FR4133,
MSP-EXP430FR6989,
I incur failure for
MSP-EXP430FR2311,
MSP-EXP430FR5994(this is the original problem i am having)
I am using
Version: 6.1.1.00022 of the Code composer studio
on a 64 bit windows platform running Windows10pro.
Any help in getting these examples to function properly would be appreciated.
Thank You.
**Attention** This is a public forum