This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2632: Empty reset vector invokes BSL doesn't work

Part Number: MSP430FR2632

Hello,

I'm using the MSP430FR2632 and would like to program the firmware using the bsl scripter. The uart is connected to a usb controller (FTDI chip). When I program the device using the bsl scripter after calling BSL from software application, all works fine! But when I have an empty device (RESET VECTOR = empty) I'm not able to program the device with the bsl scripter! An empthy reset vector should invokes the BSL if I'm right.

When I send a MASS ERASE I got no response. I perform the programming within the 10 seconds before the device goes into LPM4!

What should I do? Thanks, Ronald

 

**Attention** This is a public forum